36.4.2.7.2 Host Reception (7-Bit Addressing Mode)
The following section describes the sequence of events that occur when the module is receiving data in 7-bit Addressing mode:
- Depending on the configuration of the
Address Buffer Disable (ABD) bit, one of two methods may be used to begin
communication:
- When ABD is clear (ABD =
0
), the address buffer, I2CxADB1, is enabled. In this case, the 7-bit client address and R/W bit are loaded into I2CxADB1, with the R/W bit set (R/W =1
). The number of expected received data bytes are loaded into I2CxCNT. After these registers are loaded, software must set the Start (S) bit to begin communication. Once the S bit is set, host hardware waits for the Bus Free (BFRE) bit to be set before transmitting the Start condition to avoid bus collisions. - When ABD is set (ABD =
1
), the address buffer is disabled. In this case, the number of expected received data bytes are loaded into I2CxCNT, and the client’s 7-bit address and R/W bit are loaded into I2CxTXB. A write to I2CxTXB will cause host hardware to automatically issue a Start condition once the bus is Idle (BFRE =1
). Software writes to the Start bit are ignored.
- When ABD is clear (ABD =
- Host hardware waits for BFRE to be set, then shifts out the Start condition. Module hardware sets the Host Mode Active (MMA) bit and the Start Condition Interrupt Flag (SCIF). If the Start Condition Interrupt Enable (SCIE) bit is set, the generic I2CxIF is also set.
- Host hardware transmits the 7-bit client address and R/W bit.
- Host hardware samples SCL to determine if the client is stretching the clock, and continues to sample SCL until the line is sampled high.
- Host hardware transmits the 9th clock
pulse, and receives the ACK/NACK response from the
client.
If an ACK is received, host hardware receives the first seven bits of the data byte into the receive shift register.
If a NACK is received, hardware sets the NACK Detect Interrupt Flag (NACKIF), and:- ABD =
0
: Host generates a Stop condition, or sets the MDR bit (if RSEN is also set) and waits for software to set the Start bit to generate a Restart condition. - ABD =
1
: Host generates a Stop condition, or sets the MDR bit (if RSEN is also set) and waits for software to load a new address into I2CxTXB. Software writes to the Start bit are ignored.
If the NACK Detect Interrupt Enable (NACKIE) is also set, hardware sets the generic I2CxEIF bit.
- ABD =
- If previous data remains in the I2C
Receive Buffer (I2CxRXB) when the first seven bits of the new byte are received into the
receive shift register (RXBF =
1
), the MDR bit is set (MDR =1
), and the clock is stretched after the 7th falling edge of SCL. This allows the host time to read I2CxRXB, which clears the RXBF bit, and prevents receive buffer overflows. Once RXBF is clear, hardware releases SCL. - The host clocks in the 8th bit of the data byte into the receive shift register, then transfers the full byte into I2CxRXB. Host hardware sets the I2C Receive Interrupt Flag (I2CxRXIF) and RXBF, and if the I2C Receive Interrupt Enable (I2CxRXIE) is set, the generic I2CxIF is also set. Finally, I2CxCNT is decremented by one.
- Host hardware checks I2CxCNT
for a zero value.If I2CxCNT is nonzero (I2CxCNT !=
0
), hardware transmits the value of the Acknowledge Data (ACKDT) bit as the acknowledgement response to the client. It is up to user software to properly configure ACKDT. In most cases, ACKDT must be clear (ACKDT =0
), which indicates an ACK response.If I2CxCNT is zero (I2CxCNT =0
), hardware transmits the value of the Acknowledge End of Count (ACKCNT) bit as the acknowledgement response to the client. CNTIF is set, and host hardware either issues a Stop condition or a Restart condition. It is up to user software to properly configure ACKCNT. In most cases, ACKCNT must be set (ACKCNT =1
), which indicates a NACK response. When hardware detects a NACK on the bus, it automatically issues a Stop condition. If a NACK is not detected, the Stop will not be generated, which may lead to a stalled Bus condition. - Host hardware receives the first seven bits of the next data byte into the receive shift register.
- Repeat Steps 6 – 9 until all expected bytes have been received.