Starting with Libero® SoC v12.5, FlashPro Express supports two
modes:
Operator mode
Developer mode
Operator mode is a current flow that provides production programming. It is the
default mode and allows you to run selected actions for individual and all devices.
Developer mode allows you to:
Update jobs before running
programming.
Enable or disable chain
devices.
Load design and SPI Flash
Programming files and select different programming actions for each chain device
and SPI-Flash.
Run selected actions for individual and all devices.
You select Operator or Developer mode using the Preference dialog box (Project > Preferences). The preference is saved per user per machine on Windows and per user on
Linux. The mode preference remains the same until you change it.
The FlashPro Express mode can be switched before opening a job. If a job is opened, you
are prompted to confirm closing of the job to save the mode preference after clicking
the OK button.
After a job is opened in Developer mode, each device displays:
An info () icon with device specific
data.
Design icon (). The per-device selected
action appears next to the icon if the Run selected action for all
devices option is unselected.
SPI Flash icon () if SPI Flash programming is available
for the device. The per-device selected SPI Flash action appears next to the
icon if the Run selected action for all devices option is
unselected.
Configure button () providing a menu
of configuration options based on the device. The configure button is enabled
when no programming action is running.
The following list describes Developer mode features:
Device configuration optionsFigure 15-26. Device Options to Program DesignFigure 15-27. Device Options to Program Design and SPI Flash
Enable/Disable device for
programming: Allows the device to be enabled or disabled (put in “bypass”). You
must load the programming file when enabling a device that is in “bypass,” with
no programming file associated with the device or SPI-Flash. The device header
info tooltip is updated with selected programming action if enabled or “bypass”
if disabled.
Note: The job cannot
be saved if all devices are disabled or if any enabled devices do not have a
loaded programming file. If all the devices are disabled, an actions combo
box and a Run button are disabled.
Load Programming File: The option
is available for the enabled devices to load a different programming file for
the target device. FlashPro Express requires all programming files to be in the
local job folder. When the user loads a programming file from outside the job
folder, the system copies the file to the job folder and loads it for the
selected device. The user must confirm copying the programming file to the job
folder and overwriting the existing file.
Select a programming action and
configure actions and procedures per device: Allows the selection of the
programming action and configuration of the actions’ procedures. The option is
available for an enabled device that has programming file loaded, and when the
Run selected action for all devices option is
unselected.
Load SPI Flash file: Allows you
to load a different SPI Flash programming file.
Select SPI Flash Action: Allows
the selection of the programming action for the SPI Flash. The option is
available for the enabled device that has SPI Flash Programming File loaded, and
when the Run selected action for all devices option is
unselected.
Note: The standard SPI Flash flow uses a
.bin image file. When you export a FlashPro
Express job from Libero SoC, the SPI Flash image is always exported in BIN
format. You must use a .bin file for programming the
SPI Flash image unless you have a specific reason to use STP.
To program
an SPI Flash image in STP format, load the .stp
file through the Load Programming File option.
Before you load the STP file, unload any SPI Flash
.bin file previously loaded for the same
device. FlashPro Express handles the STP file as a design programming
file, so the run is logged as design programming in Tcl. For
example:
Program device selected actions:
In developer mode, when the Run selected action for all
devices check box is selected, FlashPro Express runs selected
action from the drop-down list below the check box for all enabled devices –
similar to Operator mode.Figure 15-28. Run One Action for All
Chain DevicesWhen the Run selected action for all devices check
box is unselected, the actions drop-down list is disabled. FlashPro Express runs
the programming actions for the enabled device and SPI Flash, as selected
uniquely for each device.Figure 15-29. Run Device Selected
Actions
FlashPro6 programmer internal design is updated to handle a corner case of JTAG state machine
traversal. This corner case is not observed using Libero or FlashPro Express tools, but
it needs to be fixed for integrating with other debug tools. The FlashPro6 design update
feature is added as part of the Libero or FlashPro Express software flow to detect the
current design version of the attached programmer and trigger an update if you choose
to. This update is possible only in Developer mode. Operator mode does not support this
feature. The tool displays a warning message in the following two scenarios:
If you choose not to proceed with
the update in Developer mode.
If the tool is in Operator mode
and the programmer design is out of date.
You can update FlashPro6 with FlashPro Express tool or with Tcl Commands.
15.1.7.1.1 Updating FlashPro6 Internal Design To New
Version In Developer Mode
In order to update FlashPro6 internal design from old version to new version in Developer
mode, you need to follow the below steps:
On connecting the FlashPro6
programmers, the Message window displays the design
information.
After executing the
RUN action, the FlashPro6 update starts.
A warning message pop up displays
all the FlashPro6 programmers that need to be updated. You can choose whether
you want the programmer to be updated with the latest design. If
Yes, the flow starts updating all the programmers
listed and then completes the action. If No, then the
flow continues with the intended action (in this case, it runs DEVICE_INFO)
along with a warning message in Warnings window.
Whenever, you choose RUN, it displays all the programmers
that need to be updated, regardless of selecting No
previously.
Note: You must not
disconnect the programmers while the update is running. If you do so, the
programmer does not get detected by the operating system. It is recommended
to contact Microchip FPGA Support to get the defective programmer
repaired.
If update passes, the programmer message shows that the update passed.
The below example shows how the
design version in FlashPro6 programmer 138013A is updated from old version 0018 to
new version 001A.
On connecting the programmer, the message window displays
the design version 0018 for FlashPro6 programmer 138013A.
Figure 15-30. Programmer Connected With
Design Version 0018After executing the RUN action, the FlashPro6 update
starts. As shown in figure below, only one programmer is out of date (that is,
138013A).Figure 15-31. Warning Message Showing The
FlashPro6 Programmer 138013A To Be Out Of Date
On choosing Yes, the FlashPro6 programmer 138013A starts
updating. If the update passes, the programmer message shows that the update passed.
Once the programmer is updated, the design version of FlashPro6 programmer 138013A
is updated to design version 001A.Figure 15-32. Programmer 138013A Showing
Design Version 001A On Successful Update
15.1.7.1.2 Updating FlashPro6 Internal Design To New
Version In Operator Mode
When a FlashPro6 programmer is out of date in Operator mode, a warning message is
displayed in Warnings window as shown in figure below. Figure 15-33. Warning Message Displayed In
Log Window Showing That Programmer Is Not Updated
The warning message states that one or more programmers require update. There are two
options to update the programmers: