9.2.19 ODT Value
(Ask a Question)If the ODT option is turned on, the ODT Value (ohm) field can be set to any one of the values in the pull- down list. The ODT Value varies with different I/O standards.
If the ODT option is turned on, the ODT Value (ohm) field can be set to any one of the values in the pull- down list. The ODT Value varies with different I/O standards.
Rev: 2026.1