16.2.5 Special
(Ask a Question)16.2.5.1 FCEND_BUFF
(Ask a Question)| Input | Output |
|---|---|
| A | Y |
| A | Y |
|---|---|
| 0 | 0 |
| 1 | 1 |
16.2.5.2 FCINIT_BUFF
(Ask a Question)| Input | Output |
|---|---|
| A | Y |
| A | Y |
|---|---|
| 0 | 0 |
| 1 | 1 |
16.2.5.3 FLASH_FREEZE
(Ask a Question)The Flash_Freeze macro is a special-purpose macro that provides information on when the chip is about to go into Flash* Freeze mode to allow the user to perform any housekeeping needed before the device enters into Flash*Freeze mode. The macro has two outputs:
- FF_TO_START—This signal goes high when the FPGA is about to go into Flash*Freeze mode.
- FF_DONE—This signal goes high when the FPGA has successfully entered Flash*Freeze mode.
For more information about this macro, see the SmartFusion 2 SoC and IGLOO 2 FPGA System Controller User Guide and the UG0444: SmartFusion2 and IGLOO2 FPGA Low-Power Design User Guide .
There is no simulation model for this macro. The two outputs remain low during simulation because Flash-Freeze is not supported during simulation.
16.2.5.4 LIVE_PROBE_FB
(Ask a Question)This is a special-purpose macro that feeds the live probe signals back to the fabric. You can connect the PROBE_A/PROBE_B signals to any unused I/O during design generation. This is useful if PROBE_A/PROBE_B cannot be brought out for debugging due to board limitations. PROBE_A and PROBE_B pins must be reserved, if LIVE_PROBE_FB macro is used. This macro is not supported in simulation.
16.2.5.5 RCOSC_1MHZ
(Ask a Question)16.2.5.6 RCOSC_1MHZ_FAB
(Ask a Question)16.2.5.7 RCOSC_25_50MHZ
(Ask a Question)16.2.5.8 RCOSC_25_50 MHZ_FAB
(Ask a Question)16.2.5.9 SYSCTRL_RESET_STATUS
(Ask a Question)This special-purpose macro checks the status of the System Controller. The RESET_STATUS output port goes high when the System Controller is in reset mode. To enable this, select the "System Controller Suspend Mode" option in the "Device Settings" under Libero's Project Settings.
- At simulation time t = 0, set
RESET_STATUS= 0. - X1 μs after observing
POWER_ON_RESET_N= 1, setRESET_STATUS= 1 to indicate that the system controller has entered suspend mode.
16.2.5.10 SYSRESET
(Ask a Question)| Input | Output |
|---|---|
| DEVRST_N | POWER_ON_RESET_N |
| DEVRST_N | POWER_ON_RESET_N |
|---|---|
| 0 | 0 |
| 1 | 1 |
16.2.5.11 XTLOSC
(Ask a Question)The crystal oscillator provides up to a 20 MHz clock signal. Physically, it requires connection to an external crystal. However, for simulation purposes the XTL pin provides a clock signal running at the desired input frequency. MODE is a two-bit configuration parameter that specifies the frequency range, as shown in the following table.
| MODE[1:0] | Frequency Range (MHz) |
|---|---|
| 00 | N/A |
| 01 | 0.032 – 0.075 |
| 10 | 0.075 – 2.0 |
| 11 | 2.0 – 20.0 |