1.3.1 Software Installation
The PLC PHY Tester PC Tool installer can be downloaded from www.microchip.com/en-us/software-library/se-plc-phy-tester-tool.
To install the software, execute the installation wizard provided. The first window allows selecting between multi-user support and current user:
The next window is the welcome window and contains some advice about tool installation:
The next window shows the user the License Agreement:
Next, select the components to install:
Finally, select the install location:
The wizard must complete without any other configuration:
The installation procedure generates a desktop link and start menu entry. Use either to start the tool. In order to be able to connect to the Microchip PLC boards, USB drivers are provided with this software. Ensure that these drivers are installed before using this tool.