1.2.6.3 BN Disconnection

This is the diagram that appears in the PRIME specification 1.3.6 showing the disconnection process initiated by a Base Node. It shows how the base node sends a disconnection request to the Service Node through another switch.

Figure 1-28. Disconnection Initiated by the Base Node
The sniffer capture shown below shows the disconnection process initiated by a Base Node. However, in this case, there is not any intermediate switch, so there are only 2 devices involved: the Base Node and the terminal or Service Node. The next image shows the disconnection process with the 2 frames involved:

In order to obtain more details, the user could go to the packet view. It is possible to find the type of messages and associate them with the previous diagram (In this case is a 4-32 connection):

  • Frame 152:
  • Frame 153:
Note: As the Negative field is equal to 1, it indicates that is a connection closing.