1.9.2 MCC Project Configuration

The following figure shows the MCC project graph of G3 Coordinator ICMPv6 Cycles application for PIC32CXMTG-EK.

Figure 1-108. MCC Project Graph of G3 Coordinator ICMPv6 Cycles for PIC32CXMTG-EK
  • Since it is an hybrid project, both G3 MAC RT and RF215 drivers are present. For PLC-only or RF-only projects, only one of them is needed.
  • The PLC PVDD Monitor service is needed to monitor the PVDD voltage of PL460 in order to disable PLC transmission in case the voltage is not in the expected range, to avoid PL460 damage. If the PVDD voltage is in the expected range the PLC transmission is enabled.
  • The PLC PHY Coupling service is needed to configure the PLC transmission parameters for the selected transmission coupling branch.
  • The USI service is needed to send/receive messages through serial interface (UART/USB) to/from external device.
  • The Console and Debug system services are used to show debug information through the serial interface.
  • The Time system service is required by both G3 MAC RT and RF215 drivers. It is used by the application to create timers.
  • The TRNG peripheral library is used by the Random service to generate random numbers, which is needed by the G3 stack. It is not mandatory due to the Random service can generate random numbers without it. However, if the MCU used has a TRNG peripheral it is recommended to use it.
  • Cryptographic and wolfCrypt libraries are used by the Security service to perform cryptographic operations needed by the G3 stack.
  • The G3 STACK folder contains all the components needed by the G3 stack.
  • The TCP/IP STACK folder contains all the TCP/IP components used by the application.
Figure 1-109. MCC Project Graph of G3 STACK Folder
  • Since it is an hybrid project, both PLC and RF G3 PALs are present. For PLC-only or RF-only projects, only one of them is needed (G3 Mode of Operation should be changed in MCC options of G3 Stack).
  • Random, Security, Queue, and Log Report services are always needed by the G3 stack.
Figure 1-110. TCP/IP Configuration Plug-in
  • TCPIP CORE is always needed by the TCP/IP stack.
  • In this application there is only one TCP/IP interface (NETCONFIG-0), which is connected to G3ADPMAC. G3ADPMAC is the interface between the TCP/IP stack and the G3 stack API (ADP).
  • IPv6 is the layer on top of the G3 stack (ADP).
  • NDP (Neighbor Discovery Protocol) module is required by the TCP/IP stack when IPv6 is used.
  • ICMPv6 is required by NDP module. It is used to send ICMPv6 Echo Requests to all devices in the network (cycles).

The following figure shows the MCC configuration of the G3 Stack.

Figure 1-111. G3 Stack MCC Configuration
  • G3 Mode of Operation: It can be changed if Hybrid PLC and RF is not needed
  • Role for G3 Node: Configured to PAN Coordinator for this application
  • For additional information about G3 stack configuration, refer to the corresponding documentation (smartenergy_g3 repository).

The following figure shows the MCC configuration of NETCONFIG.

Figure 1-112. NETCONFIG MCC Configuration
  • Multicast Enabled on this Interface: It is automatically enabled by G3ADPMAC component.
  • IPv6 Static Address and Subnet Prefix Length: IPv6 address is configured dynamically, depending on G3 PAN ID and Short Address. It is automatically disabled by G3ADPMAC component.
  • IPv6 G3-PLC network: It must be enabled when TCP/IP interface uses the G3 stack (G3ADPMAC). It is automatically enabled by G3ADPMAC component.
    • G3-PLC router: In this project it is enabled due to it is a Coordinator. It is automatically enabled by G3ADPMAC component if G3 Mode of Operation is PAN Coordinator.
  • For additional information about NETCONFIG configuration, refer to the corresponding documentation (net repository).

The following figure shows the MCC configuration of IPv6.

Figure 1-113. IPv6 MCC Configuration
  • Enable G3-PLC Support: It must be enabled when a TCP/IP interface uses the G3 stack (G3ADPMAC). It is automatically enabled by G3ADPMAC component.
    • Enable G3-PLC router support: In this project it is enabled due to it is a Coordinator. It is automatically enabled by G3ADPMAC component if G3 Mode of Operation is PAN Coordinator.
  • For additional information about IPv6 configuration, refer to the corresponding documentation (net repository).

The G3 Coordinator ICMPv6 Cycles application loads by default the configuration to use the default coupling stage of the evaluation kit (Multiband FCC + CENELEC-A for the PL460-EK). If other PLC band configuration is required, it can be easily modified in the MCC options of G3 MAC RT driver, as shown below.

Figure 1-114. PLC Band Configuration in G3 MAC RT Driver

The serial interface used to show debug information is configured in the MCC configuration of Console and Debug services. It can be UART or USB (if the device supports USB).

Figure 1-115. Console and Debug MCC Configuration

The Cryptographic Library has to be configured to support all the algorithms required by G3. The figure below shows the configuration for this example.

Figure 1-116. Crypto Configuration