1.8 SpaceWire RMAP Loopback Example
This example shows how to configure the SpaceWire peripheral to configure the RMAP module, send an RMAP command with the packet transceiver and receive the RMAP reply with the packet receiver.
Building The Application
The parent folder for all the MPLABX IDE projects for this application is given below:
Application Path: aerospace\apps\spw\spw_rmap_loopback\firmware
To build the application, refer to the table below and open the appropriate project file in MPLABX IDE.
Project Name | Description |
---|---|
sam_rh707_ek.X | SAM RH707 Evaluation Kit board |
MPLAB Harmony Configurations
Refer to the MHC project graph for the components used and the respective configuration options.
Hardware Setup
- Project sam_rh707_ek.X
Hardware Used
- SAM RH707 Evaluation Kit
- SpaceWire cable
Hardware Setup
- Connect the USB port (USB DEBUG) on the board to the computer using a micro USB cable.
- If the board embedded debugger is not used, connect the debugger probe on DEBUG connector (J5).
- Connect the two SpaceWire link on the board to each other using a SpaceWire cable.
Note : This example can also be tested with SpaceWire links configured in TTL:
- Pin configuration must be modified in Harmony Configuration to set unused pin in an other function than SpaceWire.
- Evaluation kit board must be modified like described in the user guide.
- Connect the USB port (USB DEBUG) on the board to the computer using a micro USB cable.
Running The Application
Open the Terminal application (Ex.:Tera term) on the computer.
Connect to the Virtual COM port and configure the serial settings as follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
Build and Program the application using the MPLABX IDE.
See the following message in the console.
----------------------------------------------------------- SPW RMAP loopback example ----------------------------------------------------------- Wait for both SWP link switch to run state SPW Link in Run state Initialize packet receiver to receive 1 packet(s) of 8 bytes Send SWP packet with RMAP command write with reply Wait RMAP reply Receive RMAP WRITE reply : ID = 0xabcd, with status : 0x0 RMAP write command reply with status OK Initialize packet receiver to receive 1 packet(s) of 80 bytes Send SWP packet with RMAP command read Wait RMAP reply Receive RMAP READ reply : ID = 0xabcd, with status : 0x0 Receive 64 bytes of data : 00, 01, 02, 03, 04, 05, 06, 07, 08, 09, 0A, 0B, 0C, 0D, 0E, 0F, 10, 11, 12, 13, 14, 15, 16, 17, 18, 19, 1A, 1B, 1C, 1D, 1E, 1F, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 2A, 2B, 2C, 2D, 2E, 2F, 30, 31, 32, 33, 34, 35, 36, 37, 38, 39, 3A, 3B, 3C, 3D, 3E, 3F, RMAP read command reply with status OK