2.2 Non-Inverting Amplifier

Another very common configuration is as a non-inverting amplifier. A non-inverting amplifier has an output that is greater than the input signal. The schematic for the non-inverting amplifier is shown below.

Figure 2-2. Non-Inverting Amplifier Schematic

The output of this circuit can be calculated using the following formula:

V O U T ⁢ = (   1 ⁢ +   R 2 R 1 ) * V I N