1.2.1.5.1 Abstraction Model
This module provides software abstraction of the DHCP Server module existent in any TCP/IP Stack implementation. It removes the overhead of address configuration from all other clients on the local network.

How the Library Works
To use DHCP Server, include the files dhcp_server.c, and dhcp_server.h in your project, and add or uncomment the definition "#define TCPIP_STACK_USE_DHCP_SERVER_V2" to configuration.h.
You should use a configuration tool (MCC).
The DHCP Server module will assign IP addresses to DHCP clients from the configured IP address database.
When the server receives a request from a client, the DHCP server allocates an IP address that is appropriate for the client, and sends configuration information appropriate for that client.
The IP addresses will be granted for a limited interval. DHCP clients are responsible for renewing their IP address before that interval has expired.
A DHCP client must stop using the leased address once the interval has expired, if they have not been able to renew it.