DRV_ENCX24J600_PowerMode Function
C
bool DRV_ENCX24J600_PowerMode(DRV_HANDLE hMac, TCPIP_MAC_POWER_MODE pwrMode);
Returns
- false - This functionality is not supported in this version of the driver
Description
ENCX24J600 Power Mode This function sets the power mode of the ENCX24J600.
Remarks
This functionality is not implemented in the first release.
Preconditions
The client had to be successfully opened with DRV_ENCX24J600_Open.
Parameters
Parameters | Description |
---|---|
hMac | the successfully opened handle |
pwrMode | the power mode to set |