TCPIP_TFTPS_Enable Function

C

bool TCPIP_TFTPS_Enable(TCPIP_NET_HANDLE hNet, IP_ADDRESS_TYPE ipType); 

Returns

  • true - if successful
  • false - if unsuccessful, if server open fails for this interface.

Description

This function enables the TFTP server for the specified interface and it opens the TFTP server with specific IP address TYPE.

Remarks

None.

Preconditions

The TFTPS module should have been initialized.

Parameters

ParametersDescription
hNetInterface to enable
ipTypeInterface address type. Depends on the enum type of IP_ADDRESS_TYPE bool TCPIP_TFTPS_Enable( TCPIP_NET_HANDLE hNet,IP_ADDRESS_TYPE ipType)