TCPIP_SMTP_IsPutReady Function
C
uint16_t TCPIP_SMTP_IsPutReady();
Description
Use this function to determine how much data can be written to the SMTP client when generating an on-the-fly message.
Preconditions
TCPIP_SMTP_UsageBegin() returned true on a previous call, and an on-the-fly message is being generated. This requires that TCPIP_SMTP_MailSend() was called with SMTPClient.Body set to NULL.
Returns
- The number of free bytes the SMTP TX FIFO.
Remarks
This function should only be called externally when the SMTP client is generating an on-the-fly message (i.e., TCPIP_SMTP_MailSend was called with SMTPClient.Body set to NULL).