PPP_EVENT_HANDLER Type
C
typedef void (*PPP_EVENT_HANDLER)(DRV_HANDLE hMac, PPP_EVENT event, const uint8_t* pppFrame, const void* param);
Description
Prototype of a PPP event handler. Clients can register a handler with the PPP driver.
Once an PPP event occurs the PPP driver will call the registered handler.
Parameters
hMac - driver handle (obtained by calling TCPIP_MAC_Open/DRV_PPP_MAC_Open)
event - the occurring event
pppFrame - pointer to the frame that caused the event and it's logged
param - user supplied handle parameter, Not used by the PPP module.
Remarks
Some events (PPP_EVENT_UP, PPP_EVENT_TMO_P, etc.) will have pppFrame == 0
The handler has to be short and fast. It is meant for setting an event flag, not for lengthy processing!