TCPIP_ICMPV6_EchoRequestSend Function
C
bool TCPIP_ICMPV6_EchoRequestSend(TCPIP_NET_HANDLE netH, IPV6_ADDR * targetAddr, uint16_t sequenceNumber, uint16_t identifier, uint32_t packetSize); Returns
true - if the query request was successfully sent
false - otherwise (interface not ready for transmission, allocation error, etc.)
Description
This function allows a stack client to send an ICMPv6 Echo request message to a remote host. The supplied sequence number and identifier will be used in the query message. The user will be notified by the result of the query using a notification handle registered by using the TCPIP_ICMPV6_CallbackRegister function.
Remarks
None.
Preconditions
The TCP/IP Stack is initialized and up and running. IPv6 and ICMPv6 are initialized.