TCPIP_SMTP_MailSend Function
C
void TCPIP_SMTP_MailSend(
TCPIP_SMTP_CLIENT_MESSAGE* smtpClientMessage
);
Description
This function starts the state machine that performs the actual transmission of the message. Call this function after all the fields in SMTPClient have been set.
Preconditions
TCPIP_SMTP_UsageBegin returned true on a previous call.
Parameters
Parameters | Description |
---|---|
smtpClientMessage | Pointer to a TCPIP_SMTP_CLIENT_MESSAGE structure that configures the message to send. |
Returns
None.
Remarks
The fields pointed by the smtpClientMessage have to be non-volatile until the SMTP send mail process is completed.