TCPIP_IGMP_HandlerRegister Function
C
TCPIP_IGMP_HANDLE TCPIP_IGMP_HandlerRegister(
IPV4_ADDR mcastAddress,
TCPIP_IGMP_EVENT_HANDLER handler,
const void* hParam
);
Description
This function registers an IGMP client event handler. The IGMP client module will call the registered handler when an IGMP client event (TCPIP_IGMP_EVENT_TYPE) occurs.
Preconditions
The IGMP module must be initialized.
Parameters
Parameters | Description |
---|---|
hNet | Interface handle. Use hNet == 0 to register on all interfaces available. |
handler | Handler to be called when an IGMP client event occurs. |
hParam | Pointer to be used by the application to differentiate between IGMP events. Not used by IGMP. |
Returns
Valid handle - if the call succeeds.
NULL handle - if the call failed (out of memory, for example).
Remarks
The handler has to be short and fast. It is meant for setting an event flag, not for lengthy processing.