11 (NVM) Nonvolatile Memory Control
Nonvolatile memory is separated into three categories: Program Flash Memory (PFM) including User IDs, Configuration Words, and Data Flash Memory (DFM). DFM is also referred to as EEPROM because it is written one byte at a time and the erase before write is automatic. Although User IDs are above the PFM section they are included in the PFM category because the read and write access is identical for both.
The write and erase times are controlled by an on-chip timer. The write and erase voltages are generated by an on-chip charge pump rated to function over the operating voltage range of the device.
PFM and DFM can be protected in two ways: code protection and write
protection. Code protection (Configuration bits CP for PFM and
CPD for DFM) disables read and write access through an
external device programmer. Code protection does not affect the self-write and erase
functionality whereas write protection does. Code protection write protection can only
be reset by a Bulk Erase performed by an external device programmer. A PFM Bulk Erase
clears the program space, Configuration bits, and User IDs. A Bulk Erase only clears DFM
if the CPD = 0
. When
CPD = 1
then bulk erasing DFM requires
setting the Program Counter to the DFM area before the Bulk Erase command is issued, and
then only the DFM area is cleared. See the programming specification for more details.
Write protection prevents writes to NVM areas tagged for protection by the WRTn
Configuration bits. Attempts to write a protected location will set the NVMERR bit.
PFM and Configuration Words can be accessed by either the Table Pointer or NVM controls. DFM can be accessed only by the NVM controls. The PFM access is by single byte, single word, or full sector. A sector is 256 bytes (128 PFM words). The sector memory occupies one full bank of RAM space located in the RAM bank following the last occupied GPR bank. Sector memory is also referred to elsewhere in this document as the write block holding registers. The Table Pointer accesses memory by bytes. The NVM control accesses the DFM section by bytes and the other sections by words and sectors.
The NVM controls include five independent access functions with five corresponding control bits. The controls are as follows:
- RD – Single byte/word read
- WR – single byte/word write
- SECRD – Sector read
- SECWR – Sector write
- SECER – Sector erase
The NVMADR registers determine the address of the memory region being accessed by the NVM control. The TBLPTR registers determine the address of the memory being accessed by the Table Pointer functions. The following table indicates which controls operate in each region.
Region | Address Range |
Table |
NVMCON1 | ||||
---|---|---|---|---|---|---|---|
RD | WR | SECRD | SECWR | SECER | |||
PFM |
00 0000h |
● | ● | ● | ● | ● | ● |
User IDs |
20 0000h |
● | ● | ● | ● | ● | ● |
CONFIG |
30 0000h |
● | ● | ● | ● | ||
DFM |
31 0000h |
● | ● |