1.3 Gain Error

Gain error is defined as the deviation of the measured transfer function slope from that of the ideal, after compensating for the offset error. The method used is a two-point linear intercept using histogram bins 256 and n-256. Gain error is corrected by scaling the output values. Figure 1-4 shows an example of positive gain error.

Figure 1-4. Positive Gain Error Example