16.2.3 Options
Long and short forms of options, shown in the table below as alternatives, are equivalent.
| Option | Function |
|---|---|
-A
|
Precede each symbol by the name of the input file (or archive member) in which it was found, rather than identifying the input file once only, before all of its symbols. |
-a
|
Display all symbols, even debugger-only symbols; normally these are not listed. |
-B |
The same as
--format=bsd. |
--defined-only |
Display only defined symbols for each object file. |
-u
|
Display only undefined symbols (those external to each object file). |
-f format
|
Use the output format
format, which can be
bsd, sysv or posix. The
default is bsd. Only the first character of format is
significant; it can be either upper or lower case. |
-g
|
Display only external symbols. |
--help |
Show a summary of the options to xc-dsc-nm and exit. |
-l
|
For each symbol, use debugging information to try to find a filename and line number. For a defined symbol, look for the line number of the address of the symbol. For an undefined symbol, look for the line number of a relocation entry that refers to the symbol. If line number information can be found, print it after the other symbol information. |
-n
|
Sort symbols numerically by their addresses, rather than alphabetically by their names. |
-p
|
Do not bother to sort the symbols in any order; print them in the order encountered. |
-P
|
Use the POSIX.2 standard output format
instead of the default format. Equivalent to -f posix. |
-r
|
Reverse the order of the sort (whether numeric or alphabetic); let the last come first. |
-s
|
When listing symbols from archive members,
include the index: a mapping (stored in the archive by xc-dsc-ar or xc-dsc-ranlib) of which
modules contain definitions for which names. |
--size-sort |
Sort symbols by size. The size is computed as the difference between the value of the symbol and the value of the symbol with the next higher value. The size of the symbol is printed, rather than the value. |
-t radix
|
Use radix
as the radix for printing the symbol values. It must be d for
decimal, o for octal or x for
hexadecimal. |
-V
|
Show the version number of xc-dsc-nm and exit. |