5.6.1 Implicit Alignment in Program Memory
In addition to directives that explicitly align the location counter
(such as .align, .palign, .org,
.porg, etc.), many statements cause an implicit alignment to occur
under certain conditions. Implicit alignment occurs when padding is inserted so that the
next statement begins at a valid address. Padding uses the current
.fillvalue and .fillupper values if specified;
otherwise the value zero is used.
In data memory, a valid address is available for each byte. Since no data directives specify memory in quantities of less than one byte, implicit alignment is not required in data memory.
In program memory, a valid address is available for each instruction word (3 bytes). Since data directives can specify individual bytes, implicit alignment to the next valid address is sometimes required.
The following conditions cause implicit alignment in program memory:
- Labels must be aligned to a valid address. For example, see the
following source code:
.text .pbyte 0x11 L1: .pbyte 0x22 .pbyte 0x33,0x44This generates implicit alignment as shown in the disassembly of section
.text:00000000 <.text>: 0: 11 00 00 nop 00000002 <L1>: 2: 22 33 44 .pword 0x443322Note: Two bytes of padding were inserted so that labelL1would be aligned to a valid address. - Instructions must be aligned to a valid address. For example, see
the following source code:
.text .pbyte 0x11 mov w2,w3This generates implicit alignment as shown in the disassembly of section
.text:00000000 <.text>: 0: 11 00 00 nop 2: 82 01 78 mov.w w2, w3Note: Two bytes of padding were inserted so that themovinstruction would be aligned to a valid address. - Transitions between p-type data directives
(
.pbyte,.pspace, etc). and normal data directives (.byte,.space, etc.), in either direction, are aligned to a valid address. For example, see the following source code:.text .byte 0x11 .pbyte 0x22 .pbyte 0x33,0x44This generates implicit alignment as shown in the disassembly of section
.text:00000000 <.text>: 0: 11 00 00 nop 2: 22 33 44 .pword 0x443322Note: Two bytes of padding were inserted so that the transition from normal to p-type directive would be aligned to a valid address.