10.5.5.14 Overlay Description
An overlay description provides an easy way to describe sections which are to be loaded as part of a single memory image but are to be run at the same memory address. At run time, some sort of overlay manager will copy the overlaid sections in and out of the run-time memory address as required, perhaps by simply manipulating addressing bits.
This approach is not suitable for defining sections that will be used with
the PSV window, because the OVERLAY command does not permit
individual load addresses to be specified for each section. Instead, the XC-DSC linker provides automatic support for read-only sections
in the PSV window. See Section 10.9 “Read-only Data.” for details.
Overlays are described using the OVERLAY command. The OVERLAY command is used within a SECTIONS command, like an output section description. The full syntax of the OVERLAY command is as follows:
OVERLAY [start] : [NOCROSSREFS] [AT ( ldaddr )]
{
secname1
{
output-section-command
output-section-command
...
} [:phdr...] [=fill]
secname2
{
output-section-command
output-section-command
...
} [:phdr...] [=fill]
...
} [>region] [:phdr...] [=fill]
Everything is optional except OVERLAY (a keyword), and each section must have a name (secname1 and secname2 above). The section definitions within the OVERLAY construct are identical to those within the general SECTIONS construct, except that no addresses and no memory regions may be defined for sections within an OVERLAY.
The sections are all defined with the same starting address. The load addresses of the sections are arranged such that they are consecutive in memory starting at the load address used for the OVERLAY as a whole (as with normal section definitions, the load address is optional, and defaults to the start address; the start address is also optional, and defaults to the current value of the location counter).
If the NOCROSSREFS keyword is used, and there are any references among the sections, the linker will report an error. Since the sections all run at the same address, it normally does not make sense for one section to refer directly to another.
For each section within the OVERLAY, the
linker automatically defines two symbols. The symbol __load_start_secname is defined as the starting load address of
the section. The symbol __load_stop_secname is
defined as the final load address of the section. Any characters within secname
which are not legal within C identifiers are removed. C (or assembler) code may
use these symbols to move the overlaid sections around as necessary.
At the end of the overlay, the value of the location counter is set to the start address of the overlay plus the size of the largest section.
Here is an example. Remember that this would appear inside a SECTIONS construct.
OVERLAY 0x1000 : AT (0x4000)
{
.text0 { o1/*.o(.text) }
.text1 { o2/*.o(.text) }
}
This will define both .text0 and .text1 to start at address 0x1000. .text0
will be loaded at address 0x4000, and .text1 will be loaded immediately after .text0. The following symbols will be defined:
__load_start_text0, __load_stop_text0, __load_start_text1, __load_stop_text1.
C code to copy overlay .text1 into the overlay area might look like the following:
extern char __load_start_text1, __load_stop_text1;
memcpy ((char *) 0x1000, &__load_start_text1, &__load_stop_text1 - &__load_start_text1);
The OVERLAY command is a convenience, since everything it does can be done using the more basic commands. The previous example could have been written identically as follows.
.text0 0x1000 : AT (0x4000) { o1/*.o(.text) }
__load_start_text0 = LOADADDR (.text0);
__load_stop_text0 = LOADADDR (.text0) + SIZEOF (.text0);
.text1 0x1000 : AT (0x4000 + SIZEOF (.text0)) { o2/*.o(.text) }
__load_start_text1 = LOADADDR (.text1);
__load_stop_text1 = LOADADDR (.text1) + SIZEOF (.text1);
. = 0x1000 + MAX (SIZEOF (.text0), SIZEOF (.text1));