5.4.5 .lcomm symbol, length
Reserve length
bytes for a local common
denoted by symbol
. The section and value of
symbol
are those of the new local common. The
addresses are allocated in the bss section, so that at run-time, the bytes start off
zeroed. symbol
is not declared global so it is normally
not visible to the linker.