7.1 Fatal Errors
The following errors indicate that an internal error has occurred in the assembler. Please contact Microchip Technical Support (support.microchip.com) if any of the following errors are generated:
- A dummy instruction cannot be used!
 - bad floating-point constant: exponent overflow, probably assembling junk
 - bad floating-point constant: unknown error code=error_code
 - C_EFCN symbol out of scope
 - Can’t continue
 - Can’t extend frag num. chars
 - Can’t open a bfd on stdout name
 - Case value val unexpected at line _line_ of file “_file_”
 - emulations not handled in this configuration
 - error constructing pop_table_name pseudo-op table: err_txt
 - expr.c(operand): bad atof_generic return val val
 - failed sanity check
 - filename:line_num: bad return from bfd_install_relocation: val
 - filename:line_num: bad return from bfd_install_relocation
 - Inserting “name” into symbol table failed: error_string
 - pic30_get_g_or_h_mode_value called with an invalid operand type
 - pic30_get_p_or_q_mode_value called with an invalid operand type
 - pic30_insert_dsp_writeback called with an invalid operand type
 - pic30_insert_dsp_x_prefetch_operation called with an invalid offset
 - pic30_insert_dsp_x_prefetch_operation called with an invalid operand type
 - pic30_insert_dsp_y_prefetch_operation called with an invalid offset
 - pic30_insert_dsp_y_prefetch_operation called with an invalid operand type
 - invalid segment “name”; segment “name” assumed
 - label “temp$” redefined
 - macros nested too deeply
 - missing emulation mode name
 - multiple emulation names specified
 - Relocation type not supported by object file format
 - reloc type not supported by object file format
 - rva not supported
 - rva without symbol
 - unrecognized emulation name ‘em’
 - Unsupported BFD relocation size in bytes