6.2 Contents
The listing files produced by the assembler are composed of the several elements. The example below shows a sample listing file.
The example listing file contains these elements:
- Header – contains the name of the assembler, the name of the
            file being assembled, and a page number. This is not shown if the 
-anoption is specified. - Title Line – contains the title specified by the
               
.titledirective. This is not shown if the-anoption is specified. - Subtitle – contains the subtitle specified by the
               
.sbttldirective. This is not shown if the-anoption is specified. - High-level source if the 
-ahoption is given to the assembler. The format for high-level source is:<line #>:<filename> **** <source>For example:
1:hello.c **** #include <stdio.h> - Assembler source if the 
-aloption is given to the assembler. The format for assembler source is:<line #> <addr> <encoded bytes> <source>For example:
245 000004 00 0F 78 mov w0,[w14]Note:- Line numbers may be repeated.
 - Addresses are relative to sections in this module and are not absolute.
 - Instructions are encoded in “little endian” order.
 
 - Symbol table if the 
-asoption is given to the assembler. Both, a list of defined and undefined symbols will be given. The defined symbols will have the format:DEFINED SYMBOLS <filename>:<line #> <section>:<addr> <symbol>For example:
DEFINED SYMBOLS foo.s:229 .text:00000000 _mainThe undefined symbols will have the format:
UNDEFINED SYMBOLS <symbol>For example:
UNDEFINED SYMBOLS printf 
Sample Assembler Listing File
MPLAB XC-DSC ASSEMBLY Listing:  example.1.1.s                   page 1
 Sample dsPIC Assembler Source Code
 For illustration only.
   1                    
   2                            .title " Sample dsPIC Assembler Source Code"
   3                            .sbttl " For illustration only."
   4                    
   5                            ; dsPIC registers
   6                            .equ CORCONL, CORCON
   7                            .equ PSV,2
   8                    
   9                            .section .const,psv
  10                    hello:
  11 0000 48 65 6C 6C           .ascii "Hello world!\n\0"
  11      6F 20 77 6F 
  11      72 6C 64 21 
  11      0A 00 
  12                          
  13                            .text
  14                            .global __reset
  15                    __reset:
  16                            ; set PSVPAG to page that contains "hello"
  17 000000  00 00 20           mov #psvpage(hello), w0
  18 000002  00 00 88           mov w0, PSVPAG
  19                            
  20                            ; enable Program Space Visibility
  21 000004  00 40 A8           bset.b CORCONL,#PSV
  22                            
  23                            ; make a pointer to "hello"
  24 000006  00 00 20           mov #psvoffset(hello), w0
  25                              
  26                           .end
MPLAB XC-DSC ASSEMBLY Listing:  example.1.1.s                  page 2
 Sample dsPIC Assembler Source Code
 For illustration only.
DEFINED SYMBOLS
                            *ABS*:0000000000000011 __TARGET_DIVIDE_CYCLES
                            *ABS*:0000000000000001 __C30ELF
       example.1.1.s:7      *ABS*:0000000000000002 PSV
       example.1.1.s:10     .const:0000000000000000 hello
       example.1.1.s:15     .text:0000000000000000 __reset
UNDEFINED SYMBOLS
CORCON
PSVPAG
EQUATE SYMBOLS
          __TARGET_DIVIDE_CYCLES = 0x11
                        __C30ELF = 0x1
                         CORCONL = CORCON
                             PSV = 0x2