5.9.3 .irpc symbol, value ... .endr
Evaluate a sequence of statements assigning different values to
symbol. The sequence of statements starts at the
.irpc directive and is terminated by a .endr
directive. For each character in value, symbol is set to
the character, and the sequence of statements is assembled. If no value is listed, the
sequence of statements is assembled once, with symbol set to the null string. To refer to
symbol within the sequence of statements, use
\symbol.
For example, assembling:
.irpc reg,0123
push w\reg
.endr
is equivalent to assembling:
push w0
push w1
push w2
push w3