15.5 Options
When you use the MPLAB XC-DSC archiver/librarian with command line options, the archiver insists on at least two arguments to execute: one key letter specifying the operation (optionally accompanied by other key letters specifying modifiers), and the archive name.
xc-dsc-ar [-]P[MOD
[RELPOS][COUNT]] ARCHIVE
[MEMBER...]
Most operations can also accept further
MEMBER arguments, specifying archive members. Without
specifying members, the entire archive is used.
The MPLAB XC-DSC archiver/librarian allows you
to mix the operation code P and modifier flags
MOD in any order, within the first command line
argument. If you wish, you may begin the first command line argument with a dash.
The P keyletter specifies what operation to execute; it
may be any of the following, but you must specify only one of them.
| Option | Function |
|---|---|
d | Delete modules from the archive. Specify the
names of modules to be deleted as MEMBER...;
the archive is untouched if you specify no files to delete.If you specify the v modifier, the XC-DSC archiver/librarian lists each module as it is deleted. |
m | Use this operation to move members in an
archive. The ordering of members in an archive can make a difference in how programs are linked using the library, if a symbol is defined in more than one member. If no modifiers are
used with m, any members you name in the
|
p | Print the specified members of the archive,
to the standard output file. If the v modifier is specified, show the member
name before copying its contents to standard output. If you specify no
MEMBER arguments, all the files in the
archive are printed. |
q | Append the files
MEMBER... into
ARCHIVE. |
r | Insert the files
MEMBER... into
ARCHIVE (with replacement).If one of the files named in
|
t | Display a table listing the contents of
ARCHIVE, or those of the files listed
in MEMBER..., that are present in the
archive. Normally only the member name is shown; if you also want to see the
modes (permissions), timestamp, owner, group and size, you can request that by
also specifying the v modifier. To display offsets of files in the archive,
specify the O modifier. If you do not specify a
MEMBER, all files in the archive are
listed.For example, if there is more than one file with
the same name ( |
x | Extract members (named
MEMBER) from the archive. You can use
the v modifier with this operation, to request that the
archiver list each name as it extracts it.If you do not
specify a |
A number of modifiers (MOD) may immediately follow the P
keyletter to specify variations on an operation’s behavior.
| Option | Function |
|---|---|
@
file | Read options from
file. |
a | Add new files after an existing member of the archive. If you
use the modifier a, the name of an existing archive member
must be present as the RELPOS argument,
before the ARCHIVE specification. |
b | Add new files before an existing member of
the archive. If you use the modifier b, the name of an
existing archive member must be present as the
RELPOS argument, before the
ARCHIVE specification (Same as
i). |
c | Create the archive. The specified
v is always created if it did not exist, when you requested
an update. But a warning is issued unless you specify in advance that you
expect to create it, by using this modifier. |
f | Truncate names in the archive. The XC-DSC archiver/librarian will normally permit
file names of any length. This will cause it to create archives that are not
compatible with the native archiver program on some systems. If this is a
concern, the f modifier may be used to truncate file names
when putting them in the archive. |
i | Insert new files before an existing member of
the archive. If you use the modifier i, the name of an
existing archive member must be present as the
RELPOS argument, before the
ARCHIVE specification (Same as
b). |
l | This modifier is accepted but not used. |
N | Uses the
COUNT parameter. This is used if there are
multiple entries in the archive with the same name. Extract or delete instance
COUNT of the given name from the
archive. |
O | Display member offsets inside the archive. Use together with
the t option. |
o | Preserve the original dates of members when extracting them. If you do not specify this modifier, files extracted from the archive are stamped with the time of extraction. |
P | Use the full path name when matching names in
the archive. The XC-DSC archiver/librarian
cannot create an archive with a full path name (such archives are not
POSIX compliant), but other archive
creators can. This option will cause the archiver to match file names using a
complete path name, which can be convenient when extracting a single file from
an archive created by another tool. |
s | Write an object-file index into the archive,
or update an existing one, even if no other change is made to the archive. You
may use this modifier flag either with any operation, or alone. Running
xc-dsc-ar s on an archive
is equivalent to running xc-dsc-ranlib on it. |
S | Do not generate an archive symbol table. This
can speed up building a large library in several steps. The resulting archive
cannot be used with the linker. In order to build a symbol table, you must omit
the S modifier on the last execution of the archiver, or you
must run ranlib on the archive. |
u | Normally, xc-dsc-ar r... inserts all files listed into the archive. If
you would like to insert only those of the files you list that are newer than
existing members of the same names, use this modifier. The u
modifier is allowed only for the operation r (replace). In
particular, the combination qu is not allowed, since checking
the timestamps would lose any speed advantage from the operation
q. |
v | This modifier requests the verbose version of
an operation. Many operations display additional information, such as, file
names processed when the modifier v is appended. |
V | This modifier shows the version number of the XC-DSC archiver/librarian. |