3.2.1.2 -ad
-ad omits debugging directives from the listing. This
is useful if a compiler that was given a debugging option generated the assembly source
code. The compiler-generated debugging directives will not clutter the listing. The
example below shows a listing using both the d and h
suboptions. Compared to using the h sub-option alone (see the next
section), the listing is much cleaner.
Listing File Generated with -alhd Command Line Option
1 .file "example2.3.c"
2 .text
3 .align 2
9 .global _main ; export
10 _main:
1:example2.3.c **** extern int ADD (int, int);
2:example2.3.c ****
3:example2.3.c **** int
4:example2.3.c **** main(void)
5:example2.3.c **** {
16 .set _ ___PA_ ___,1
17 000000 00 00 FA lnk #0
18
6:example2.3.c **** return ADD(4, 5);
20 000002 51 00 20 mov #5,w1
21 000004 40 00 20 mov #4,w0
22 000006 00 00 02 call _ADD
22 00 00 00
7:example2.3.c **** }
29
30 00000a 00 80 FA ulnk
31 00000c 00 00 06 return
32 .set _ ___PA_ ___,0
37
38 .end