5.4.2 .comm symbol, length [, algn]
Declares a common symbol named symbol.
When linking, a common symbol in one object file may be merged with a defined or common
symbol of the same name in another object file. If the linker does not see a definition for
that symbol, then it will allocate length bytes of
uninitialized memory. If the linker sees multiple common symbols with the same name, and
they do not all have the same size, the linker will allocate space using the largest
size.
If algn is specified, it is the address
alignment required for symbol. The requested alignment must be a power of two.
algn is supported when the object file format is
ELF; otherwise, it is ignored.