12.5 Locating a Constant at a Specific Address in Program Memory [DD]
In this example, the constant table is located at a
specific address in program memory. When a constant is specifically placed at an address in
program memory, it must be placed in its own PSV section using the
space(psv) attribute. If a device has only one PSV page (16K instruction words
or less), the (psv) section and (auto_psv) section will
share the same PSV page by default.
- It is not possible to place a constant at a specific address in Program Memory using
the
space(auto_psv)attribute. Only thespace(psv)attribute may be used to perform this task. - On dsPIC33A devices, only the
address()attribute is used, and the address must be divisible by 4. Helper functions are not required.
The __builtin_tbladdress() helper function can be used to
find the address of a constant stored in program memory. The __psv__
access qualifier is used to specify compiler-managed access.
#include "stdio.h"
#include "xc.h"
__psv__ const unsigned __attribute__ ((space(psv), address (0x2000))) table[10] = {0, 1, 2, 3, 4, 5, 6, 7, 8, 9};
int main(void)
{
unsigned sum=0, u;
long addr;
/* compute the address of table and print it */
addr = __builtin_tbladdress(table);
/* print the address of table */
printf ("table[] is stored at address 0x%lx\n", addr);
/* sum the values in table[] */
for (u=0; u<10; u++) {
sum += table[u];
}
/* print the sum */
printf ("sum is %d\n", sum);
}
The equivalent constant definition for the array table in assembly
language appears below. The .align directive is optional and represents
the default alignment in program memory. Use of * as a section name causes
the assembler to generate a unique name based on the source file name.
.section *,address(0x2000),psv
.global _table
.align 2
_table:
.word 0,1,2,3,4,5,6,7,8,9
In order to allocate table in data memory, the space(psv)
attribute could be changed to space(data). In this case, the specified
address would be a data memory address. In the absence of a space attribute, the keyword
const directs the C compiler to allocate the variable in the same space
as other compiler constants. Constants are allocated in program memory by default, or in
data memory if the constants-in-data memory model is selected.