3.2 Setting Up the Programmer
For programming devices, you can use any of the supported tools (see Programming Tools Supported). Refer to the online help of the selected tool (for example, MPLAB ICD 4, PICkit 4, etc.) for information on programming a device.
- Using the Family drop-down menu, select the family of the device you
wish to program, then use the Device drop-down menu to select the device. Or use the
Device drop-down menu directly to select the device.Note: Selecting the Recently Used option from the Family menu lists the latest 10 devices used in the Device menu.
Figure 3-2. Recently Used - Click Apply to configure the IPE to the current device (for example, Target Memory Views, checksum).
- Connect the development tool to the PC and attach the appropriate target board, device and power. Refer to the tool’s online help for additional instructions and information on connecting to target boards, etc.
- Use the Tool drop-down menu to select the tool you want to use. If
more than one development tool is connected to the PC, select the one you wish to
use.
Figure 3-3. Select Tool - Click the Connect button (next to the Tool name) to establish a connection between the IPE and the tool.
- When the tool is connected, any messages or errors related to this
tool will be displayed in the Output window (refer to the following figure).
Figure 3-4. Output Window - After the tool is successfully connected, proceed to the next chapter to program the device with the IPE.