3.4.4 Environment
Environments allow you to save settings, so that all of the same settings can be reloaded in another programming session. Environments are supported, under all tools, as either .pen files or .pm3 files.
From the Advanced Mode dialog, click Environment to display the available settings.
| Setting | Description |
|---|---|
| Note: The options available will vary depending on the device and too selected. The following may not show every possible option. | |
| Create Environment Tab | |
| Environment Information | |
| Name | Enter a name for the environment. |
| .pm3 file | For MPLAB device programmers, select this type of. file. |
| .pen file | For MPLAB debuggers or emulators, select this type of file. |
| Description | Enter the description for the environment. |
| Misc Files | Add or remove other files used in the
environment, for example, data sheets, instructions, etc. Multiple files can be selected. |
| SQTP File | Browse or enter the SQTP file name used in the environment. |
| Save to PM3 Card | Saves the environment file to a MPLAB PM3 SD card destination. See ADD LINK TO REFERENCE SECTION Save Firmware into PM3 SD Card for additional information on saving multiple operating system firmware to the SD card. |
| Save to PC | Saves the environment file to a destination on the PC. |
| Copy | Opens the Copy Environment dialog to select source and destination for copying the environment. |
| Browse Environments Tab | |
| Browse on: | Select either PC or MPLAB PM3 Card. |
| PC | When the PC is selected, it opens the PM3 Environment file selection browser for you to select an environment to load into the MPLAB PM3. |
| MPLAB PM3 Card | When this option is selected, it opens
the PM3 Card browser for you to select an environment from the files on
the PM3 Card. In the browser, you can: View the properties of the PM3 SD Card. Format the PM3 SD card. Select an environment to load into the MPLAB PM3; the information displays in the Environment Settings window. Select an environment to delete from the PM3 Card. Select an environment to view information; information displays in the Environment Settings window. |
| Environment Information | Displays information related to the selected environment file such as Name, Path and Environment Description. From here, you can select to clear the information or load the environment into the MPLAB PM3. |