4.2.2 File>Import
The Import menu item allows you to import various files into the IPE. By default, these commands are not available in Production Mode. However, in Advanced Mode, an authorized user can change the default states of this feature for the Production Mode.
- File>Import>Environment – select to import (load) the environment (*.pen or .pm3 file).
- File>Import>Hex – select to import a hexadecimal file (*.hex).Note: If using a Hex file in the IPE and the file is modified using Notepad, MPLAB X IDE, etc., outside the IPE, the following message displays:

- File>Import>Multiple Hex –
select to import multiple hexadecimal files (*.hex).Note: If Hex files were generated for individual memories for EEPROM, Flash, etc., these Hex files can be imported in the MPLAB IPE. These files are loaded in a FIFO (first in, first out) manner. When loaded into the IPE, the contents are loaded into the respective memory regions of the selected device. If memory regions overlap, a warning message displays in the Output window.
From the Hex File Selection dialog, click the + button to browse and add files, or click the - button to remove a file. Select Load to import the files.
- File>Import>SQTP – select to load the SQTP file (*.num file).