6.1.2.1 Building and Running the TCP Server Application
Building the Application
To build this application, open the project file
(
Running the Application
apps\tcp_server\firmware\tcp_server_sam_e54_xpro_wincs02.X/) in
MPLAB X IDE. For more details on opening the project file in MPLAB X IDE, refer to the
Opening the
Project File. The following table provides details on the project file.| Project Name | Description |
|---|---|
tcp_server_sam_e54_xpro_wincs02.X |
|
- Mount the WINCS02 Add On Board on SAM E54 Xplained Pro evaluation kit at respective header. For more details about the boards placement in the SAM E54 X-plained host board, see Figure
- Connect the debugger USB port on the SAM E54 Xplained Pro evaluation kit to computer using a micro-USB cable.
- Open the project and launch MCC Harmony3.
- Configure Home-AP credentials for STA mode, using the WINCS02 Wi-Fi
configuration options. For more details about the Wi-Fi settings configuration,
See Sta_Mode. Note: Update the SYS_RNWF_NET_NO_OF_CLIENT_SOCKETS macro in sys_rnwf_net_service.h to reflect the number of client sockets the system can manage in server mode. (supports max 5 clients).
-
Generate the code as illustrated below.
Figure 6-5. Generating the Code 
- Build and program the code to the
hardware using MPLABX IDE.
Figure 6-6. Programming the Board 
- Open the Terminal application
(for example, Tera Term or PuTTY) on the PC
Connect to the "EDBG Virtual COM Port" and configure the serial settings as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- As the board boots up, it will connect to Home-AP and print the IP address obtained. After establishing a successful TCP server-client connection, the application will continue listening on the socket number configured for incoming messages and then write them back to the client connected.
-
Figure 6-7. TCP Server - Serial Logs