8.6.7.2 Mailbox Organization
The CAN module has 8 buffers, also called channels or mailboxes. An identifier that corresponds to the CAN identifier is defined for each active mailbox. Message identifiers can match the standard frame identifier or the extended frame identifier. This identifier is defined for the first time during the CAN initialization, but can be dynamically reconfigured later so that the mailbox can handle a new message family. Several mailboxes can be configured with the same ID.
Each mailbox can be configured in Receive or in Transmit mode independently. The mailbox object type is defined in the MOT field of the Message Mode register (CAN_MMRx).