8.2.4.8 Hash Addressing
The hash address register is 64 bits long and takes up two locations in the memory map. The least significant bits are stored in hash register bottom and the most significant bits in hash register top.
The ‘Unicast Hash Enable’ and the ‘Multicast Hash Enable’ bits in the EMAC_NCFGR enable the reception of hash matched frames. The destination address is reduced to a 6-bit index into the 64-bit hash register using the following hash function. The hash function is an exclusive or of every sixth bit of the destination address.
hash_index[5] = da[5] ^ da[11] ^ da[17] ^ da[23] ^ da[29] ^ da[35] ^ da[41] ^ da[47]
hash_index[4] = da[4] ^ da[10] ^ da[16] ^ da[22] ^ da[28] ^ da[34] ^ da[40] ^ da[46]
hash_index[3] = da[3] ^ da[09] ^ da[15] ^ da[21] ^ da[27] ^ da[33] ^ da[39] ^ da[45]
hash_index[2] = da[2] ^ da[08] ^ da[14] ^ da[20] ^ da[26] ^ da[32] ^ da[38] ^ da[44]
hash_index[1] = da[1] ^ da[07] ^ da[13] ^ da[19] ^ da[25] ^ da[31] ^ da[37] ^ da[43]
hash_index[0] = da[0] ^ da[06] ^ da[12] ^ da[18] ^ da[24] ^ da[30] ^ da[36] ^ da[42]
da[0] represents the least significant bit of the first byte received, that is, the multicast/unicast indicator, and da[47] represents the most significant bit of the last byte received.
If the hash index points to a bit that is set in the hash register, then the frame is matched according to whether the frame is multicast or unicast.
A multicast match is signalled if the ‘Multicast Hash Enable’ bit is set. da[0] is 1 and the hash index points to a bit set in the hash register.
A unicast match is signalled if the ‘Unicast Hash Enable’ bit is set. da[0] is 0 and the hash index points to a bit set in the hash register.
To receive all multicast frames, the hash register should be set with all ones and the ‘Multicast Hash Enable’ bit should be set in the EMAC_NCFGR.