Case 2: Secure SAM-BA Monitor is still
available (the “MON_DIS” word is zeroed in the Boot Configuration Packet - not recommended
for systems in production)
Disable the access to the external
boot memory (Chip Select pin, Card Detect pin, etc., depending on the chosen boot
memory) to prevent its access by the ROM code on the next reboot.
Connect a USB cable on the USB device
port, or on the UART used as SAM-BA Monitor console terminal.