22.3.2.4.4.5 Input Mode 5: Stop all Outputs, Execute Dead Time while Fault Active
When Input mode 5 is used, both input A and input B give the same functionality:
The input event stops the outputs and starts on the opposite dead-time if it occurs during an on-time. If the event occurs during a dead-time, it will continue until the next on-time should start, but instead, it will jump to the next dead-time. As long as the input event is active, alternating dead-times will occur. When the input event stops, the ongoing dead-time will finish and the next on-time will continue in the normal flow.