9.5.4 Stack and Stack Pointer
The stack is used for storing return addresses after interrupts and subroutine calls. Also, it can be used for storing temporary data. The Stack Pointer (SP) always points to the top of the stack. The SP is defined by the Stack Pointer bits in the Stack Pointer register (CPU.SP). The CPU.SP is implemented as two 8-bit registers that are accessible in the I/O memory space.
Data is pushed and popped from the stack using the
PUSH and POP instructions. The stack grows from higher
to lower memory locations. This implies that pushing data onto the stack decreases the SP,
and popping data off the stack increases the SP. The Stack Pointer is automatically set to
the highest address of the internal SRAM after Reset. If the stack is changed, it must be
set to point above address 0x2000, and it must be defined before any subroutine calls are
executed and before interrupts are enabled.
During interrupts or subroutine calls the
return address is automatically pushed on the stack as a word pointer and the SP is
decremented by '2'. The return address consists of two bytes and the Least Significant Byte
is pushed on the stack first (at the higher address). As an example, a byte pointer return
address of 0x0006 is saved on the stack as 0x0003 (shifted one bit to the right), pointing
to the fourth 16-bit instruction word in the program memory. The return address is popped
off the stack with RETI (when returning from interrupts) and
RET (when returning from subroutine calls) and the SP is incremented
by two.
The SP is decremented by '1' when data is
pushed on the stack with the PUSH instruction, and incremented by '1' when
data is popped off the stack using the POP instruction.
To prevent corruption when updating the Stack Pointer from software, a write to SPL will automatically disable interrupts for up to four instructions or until the next I/O memory write.