2.2.1 Starting Conversion
In Single Conversion mode, a conversion is triggered by writing a
'1' to the ADC Start Conversion bit (STCONV) in the
Command register (ADC.COMMAND). This bit is '1' as long as
the conversion is in progress, and will be cleared when the conversion is
completed. If a different input channel is selected while a conversion is in
progress, the ADC will finish the current conversion before changing the
channel.
In Free-Running mode, the first conversion is started by writing the
STCONV bit to '1' in ADC.COMMAND. A new conversion cycle is
started immediately after the previous conversion cycle has completed. The
Result Ready flag (RESRDY) in the Interrupt Flag register (ADC.INTFLAG) is
set.
If the Result Ready Interrupt Enable (RESRDY) bit in the Interrupt
Control (ADC.INTCTRL) register and the Global Interrupt Enable bit in the
CPU Status register (CPU_SREG.I) are '1', the Result Ready
Interrupt vector will be executed.
The RESRDY Interrupt flag in ADC.INTFLAG will be set, even if the specific interrupt is disabled, allowing software to check for finished conversion by polling the flag. A conversion can thus be triggered without causing an interrupt.
Alternatively, a conversion can be triggered by an event. This is
enabled by writing a '1' to the Start Event Input bit
(STARTEI) in the Event Control register (ADC.EVCTRL). Any incoming event
routed to the ADC through the Event System (EVSYS) will trigger an ADC
conversion. This provides a method to start conversions at predictable
intervals or at specific conditions. The event trigger input is edge
sensitive. When an event occurs, STCONV in ADC.COMMAND is set. STCONV will
be cleared when the conversion is complete.