4.2.2 RX - PMD Transceiver RX Pin
The RX pin is a high-speed low-voltage 2.5V/3.3V output from the transceiver to the microcontroller Digital PHY. In the TRANSMITTING and NORMAL (receive) states, the RX pin indicates changes in the detected polarity of the differential voltage at the TRXN/TRXP following an inverted return-to-zero (RZI) scheme. A low pulse is output on the RX pin each time the detected differential voltage at the TRXP/TRXN pins switch polarity. Together with the ED pin, the RX pin is used to signal activity detection and collision detection.
When the transceiver is in the CONFIGURATION state, the RX pin, together with the ED pin, acts as a Clause 22 MII Management (MIIM) interface. In this mode, the RX pin takes the role of the MIIM Data Clock (MDC) input of the management interface.
The RX pin also reflects the LOW_POWER state of the transceiver to the Digital PHY. The RX pin is internally pulled up to the continuous VIO power supply by a 55 kΩ resistor and will therefore be high when in a low power state. The device will actively drive the RX pin low to signal the Digital PHY when a wake event is detected. This falling edge of the RX pin can therefore be used to wake the microcontroller from a low power state. During reset, this pin is also pulled low because the transceiver state machine starts in the low power wake state.