5.2 Ethernet 10BASE‑T1S
The status of the Ethernet line TRXP and TRXN pins depends on the current state of the transceiver state machine. While in RESET, CONFIGURATION and LOW-POWER states, the pins will be high impedance. When the transceiver is in TRANSMIT state, the TX pin controls the polarity of the differential voltage pulses driven by the PMD transceiver onto the TRXP/TRXN pins. Similarly, the RX pin reflects changes in the polarity of the differential voltage detected on the TRXP/TRXN pins when in the NORMAL or TRANSMIT states.