5.3 OPEN Alliance Wake/Sleep

The OPEN Alliance defines a mechanism with which to put the device into a low power state to reduce power consumption. In this state, the switchable power supply is turned off and only the power supply on the VIO pin is active.

The wake-up events include a Wake-Up Pulse (WUP) on the 10BASE‑T1S transmission line and a level change on the TX line of the 3‑pin interface if the switchable power supply VCC is active. After waking, the wake source is saved in registers so that the accompanying microcontroller can determine the wake source. The wake source will remain in memory even if the switchable supply voltage is disabled.

A WUP on the MDI is comprised of a sequence of SUSPEND symbols, a Wake Up Tone (WUT), a series of COMMIT symbols, followed by End-of-Stream / End-of-Stream-Okay (ESD/ESDOK) termination symbols. The WUT is a signal of 12 periods of a 625 kHz tone.

A wake event is also triggered by a falling edge on the TX pin of the 3‑pin interface while the device is in low power mode. This edge is triggered by the microcontroller when it drives the TX line low to ground.

The device will exit the low power state within 35 µs of receiving the corresponding signal. Upon waking, the device will drive the RX pin of the 3‑pin interface low and drive the ED pin low within 1 ms of stabilized power. If the transceiver does not receive a reset command from the 3‑pin interface within the time specified in the time defined by the OPEN Alliance 10BASE-T1S Sleep/Wake-up Specification after waking, the device will return to the low power state.