5.2.9 Oscillator Calibration Constants
Some Baseline and Mid-range devices have an oscillator calibration constant pre-programmed into their program memory. This constant can be read and written to the OSCCAL register to calibrate the internal RC oscillator.
On some Baseline PIC devices, the calibration constant is stored as a
movlw
instruction at the top of program memory, e.g., the
PIC10F509 device. On Reset, the program counter is made to point to this
instruction and it is executed first before the program counter wraps around to
0x0000, which is the effective Reset vector for the device. The default runtime
startup routine (see Runtime Startup Code) will automatically include code to load the OSCCAL register
with the value contained in the W register after Reset on such devices. No other
code is required.
For other chips, such as PIC12F629 device, the oscillator constant is also
stored at the top of program memory, but as a retlw
instruction.
The compiler’s startup code will automatically generate code to retrieve this
value and perform the configuration. This value can also be read at runtime by
calling __osccal_val()
, whose prototype is provided in
<xc.h>. For example:
unsigned char calVal;
calVal = __osccal_val();
Loading of the calibration value at startup can be turned off via the
-mno-osccal
option (see Osccal Option).
retlw
instruction cannot be programmed and subsequent calls
to __osccal_val()
will not work. If you wish to test code
that calls this function on an ICE, you must program a retlw
instruction at the appropriate location. Remember to remove this instruction when
programming the actual part so you do not destroy the calibration value.Legacy projects can use the macro _READ_OSCCAL_DATA()
,
which maps to the __osccal_val()
function.