5.8.1.3 Reentrant And Nonreentrant Specifiers
The __reentrant
and __nonreentrant
function specifiers indicate the function model (stack) that should be used for that
function’s stack-based variables (auto and parameters), as shown in the Table 5-11 table. The aliases __software
and __compiled
,
respectively, can be used if you prefer. You would only use these specifiers if the default
allocation is unacceptable.
Specifier | Allocation for Stack-based variables |
---|---|
__compiled ,
__nonreentrant | Always use the compiled stack; functions are nonreentrant |
__software ,
__reentrant | Use the software stack, if available; functions are reentrant |
The following shows an example of a function that will always be encoded as reentrant.
__reentrant int setWriteMode(int mode)
{
accessMode = (mode!=0);
reutrn mode;
}
These specifiers override any setting indicated using the
-mstack
option (see Stack Option). If neither function
specifier is used with a function and the -mstack
option is not specified
(or specified as hybrid), then the compiler will choose the stack to be used by that
function for its stack-based variables.
The __reentrant
specifier only has an effect if the
target device supports a software stack. In addition, not all functions allow reentrancy.
Interrupt functions must always use the compiled stack, but functions they call may use the
software stack. Functions encoded for Baseline and Mid-range devices always use the
nonreentrant model and the compiled stack.
Repeated use of the __software
(__reentrant
) specifier will increase substantially the size of the
software stack leading to possible overflow. The size of the software stack is not
accurately known at compile time, so the compiler cannot issue a warning if it is likely to
overwrite memory used for some other purpose.
See Data Stacks for device specific information relating to the data stacks available on each device.