6.1.1.2 Bank And Page Selection
The BANKSEL()
pseudo instruction can be used to generate
instructions to select the bank of the operand specified. The operand should be the symbol
or address of an object that resides in the data memory.
Depending on the target device, the generated code will either contain one
or more bit instructions to set/clear bits in the appropriate register, or use a
movlb
instruction (in the case of enhanced mid-range or PIC18 devices).
As this pseudo instruction can expand to more than one instruction on mid-range or baseline
parts, it should not immediately follow a btfsx
instruction on those devices. For example:movlw 20
BANKSEL(_foobar) ;select bank for next file instruction
movwf BANKMASK(_foobar) ;write data and mask address
Note: The manual masking of addresses used as instruction operands
(for example using the
BANKMASK()
or PAGEMASK()
macros or ANDing the operand with a mask) is not necessary when using the
-Wl,--fixupoverflow
option and any of the
ignore
, warn
, or lstwarn
arguments.In the same way, the PAGESEL()
pseudo instruction can be
used to generate code to select the page of the address operand. For the current page, you
can use the location counter, $
, as the operand.
Depending on the target device, the generated code will either contain one
or more instructions to set/clear bits in the appropriate register, or use a
movlp
instruction in the case of enhanced mid-range PIC devices. As the
directive could expand to more than one instruction, it should not immediately follow a
btfsx
instruction. For
example:fcall _getInput
PAGESEL $ ;select this page
This directive is accepted when compiling for PIC18 targets but has no effect and does not generate any code. Support is purely to allow easy migration across the 8-bit devices.