5.4.4.1 Absolute Objects In Data Memory

Any object that has static storage duration and file scope can be placed at an absolute address in data memory; thus, all objects except for static objects defined inside a function and stack-based objects can be made absolute.

For example, the following declaration:
volatile unsigned char Portvar __at(0x06);
will declare a variable called Portvar located at 06h in the data memory. Note that the __at() construct can be placed before or after the variable identifier in the definition.
Note: Defining absolute objects can fragment memory and can make it impossible for the linker to position other objects. If absolute objects must be defined, try to place them at either end of a memory bank so that the remaining free memory is not fragmented into smaller chunks.

The compiler will mark storage for absolute objects as used if the address is within general-purpose RAM (GPR). Note that address 0 (zero) is not considered to be part of the GPR for PIC18 devices. Taking the address of an object at this address would yield a NULL pointer, and the compiler often uses this location for internally-defined objects. You should not place absolute objects at address 0.

No checks are made for the overlap of absolute variables with other absolute variables. There is no harm in defining more than one absolute variable to live at the same address if this is what you require. No warning will be issued if the address of an absolute object lies outside the memory of the device or outside the GPR defined by the linker classes.

Absolute variables in RAM cannot be initialized when they are defined and are not cleared by the runtime startup code. After defining absolute variables, assign them an initial value at a suitable point in your main-line code, if required.

Objects should not be made absolute to force them into common (unbanked) memory. Always use the __near qualifier for this purpose (see Near Type Qualifier).

When defining absolute bit variables (see Bit Data Types And Variables), the address specified must be a bit address. A bit address is obtained by multiplying the byte address by 8, then adding the bit offset within that bit. For example, to place a bit variable called mode at bit position #2 at address 0x50, use the following:
bit mode __at(0x282);
When compiling for an Enhanced Mid-range PIC device, the address specified for absolute objects can be either a conventional banked memory address or a linear address. As the linear addresses start above the largest banked address, it is clear which type of address has been specified. In the following example:
int input[100] __at(0x2000);
it is clear that input should be placed at address 0x2000 in the linear address space, which corresponds to address 0x20 in bank 0 RAM in the conventional banked address space.