3.6.7.2 d: Preprocessor Debugging Dumps Option
The -dletters
option has the preprocessor produce debugging
dumps during compilation as specified by letters
. This option
should be used in conjunction with the -E
option.
The
-dM
option generates a list of #define
directives
for all the macros defined during the execution of the preprocessor, including
predefined macros. These will indicate the replacement string if one was defined. For
example, the output might
include:#define _CP0_BCS_TAGLO(c,s) _bcsc0(_CP0_TAGLO, _CP0_TAGLO_SELECT, c, s)
#define PORTE PORTE
#define _LATE_LATE1_LENGTH 0x00000001
#define _IPC22_w_POSITION 0x00000000
You can use this option to show those
macros which are predefined by the compiler or header files.The acceptable letter arguments to -d
are tabulated below.
Letter | Produces |
---|---|
D |
Similar output to -dM but lacking predefined macros.
The normal preprocessor output is also included in this output. |
M |
Full macro output, as described in the main text before this table. |
N |
Similar output to -dD but only the macro names are
output with each definition. |