8.2.4 boot_lock_fuse_bits_get Macro
Read the lock or fuse bits.
Include
<avr/boot.h>
Prototype
int boot_lock_fuse_bits_get(unsigned int address);
Remarks
This macro returns the value of the lock or fuse bits at the specified
address. The address argument can be one of
GET_LOW_FUSE_BITS, GET_LOCK_BITS,
GET_EXTENDED_FUSE_BITS, or GET_HIGH_FUSE_BITS. The
bits returned are the physical values, this if a bit position was 0, it impiles that the
corresponding location was programmed.
Example
#include <avr/boot.h>
int main(void)
{
boot_lock_bits_set(_BV(BLB11)|_BV(BLB12));
}