7.4.2 Absolute Addressing
Variables and functions can be placed at an absolute address by using the
__at() construct. Stack-based (auto and parameter)
variables cannot use the __at() specifier.
Example
int scanMode __at(0x200);
const char keys[] __at(124) = { ’r’, ’s’, ’u’, ’d’};
__at(0x1000) int modify(int x) {
return x * 2 + 3;
}Differences
The legacy syntax used by MPLAB XC8 when targeting PIC MCUs has been an
@ symbol to specify an absolute address.
When targeting AVR MCUs, MPLAB XC8 has used the address attribute to
specify an object’s address. This attribute has also been used by the other
compilers.
Migration to the CCI
Avoid making objects and functions absolute if possible.
int scanMode @ 0x200;change this
to:int scanMode __at(0x200);int scanMode __attribute__((address(0x200)));to:int scanMode __at(0x200);Caveats
If building for PIC device using MPLAB XC8 and the __at() and
__section() specifiers have both been applied to an object, the
__section() specifier is currently ignored.
The MPLAB XC32 compiler for PIC32C/SAM devices supports only 4-byte aligned absolute addresses.